Other Parts Discussed in Thread: TS5A22362 Hello,
I am using the TS5A22362 for switching audio audio from a Tablet to an Audio Amplifier or to a 3.5mm Plug.
Since the 3.5mm plug has 4 signals, I'm using two TSA22362 for switching the four signals.…
Other Parts Discussed in Thread: TS5A22362 , TS5A22364 Hello
TS5A22362's datasheet was decribed as shown below.(Datasheet 15 Page)
Does this block is a block of TS5A22362 right??
Other Parts Discussed in Thread: TS5A22362 , TS5USBA224 Hola,
Does TS5A22362 support UART TX/RX signal, due to connect to debug interface?
The application block diagram is as below:
Part Number: TS3L501E Other Parts Discussed in Thread: TS5A22362
Hi,
One of our design circuit uses TS3L501E to switch b/w two Ethernet networks. I have the following questions:
The post here says: " Yes, driving the ethernet lines while the device…
Other Parts Discussed in Thread: TS5A22362 Hola Adam,
I have one more question:
We will use TS5A22362 to headphone and speaker output.
Does TS5A22362 support audio amplifier output signal, if audio source is 3.6W RMS output?
Audio amplifier chip is TFA989x…
Yaita,
The TS5A22362 has a data rate of approximately 34Mbps. This was calculated from the following...
C~=2*B where C -> data rate and B -> Max Bandwidth
The Max Bandwidth for the TS5A22362 is 17MHz, therefore 2*17 = 34Mbps.
Since the data…
Other Parts Discussed in Thread: TS5A22362 , TS5A22364 , TS3A227E Hello,
I'm posting this for a local customer:
"Quick question on this analog switch TS5A22362 -
I was looking for whether the NC connection on this analog switch stays ‘connected…
Part Number: SN3257-Q1 Other Parts Discussed in Thread: TS5A22362 , TS5A22364 , Hi team.
Could sn3257 support analog audio signal? If not, which part is the suitable?
Thanks
Jiawei
Part Number: TS5A22364 Other Parts Discussed in Thread: TS5A22362 Hi, TI Support Team
Inquiries were received while the customer was using the following products.
- TS5A22364YZPR
TI Audio Switch.pdf
As shown in the attached data, there is a difference…