Part Number: TS5A3153 Hello Respected
This is Thilaga from Flex We are currently working with one of our manufacturing plants to collect below information
Site: Zhuhai
Please provide us the MSL data for the below parts
MPN
MFR_DSCA
MSL…
Hi Artem,
Yes you can, but the on capacitance will most likely short well before the C_DS capacitor, so in general this can be assumed to be an open circuit within the operating parameters of the switch. And yes bandwidth is realistically the f_pole…
Part Number: TS5A3153 Hi Expert,
I didn't see Tj information in datasheet, could you help to share it with me?
what's the maximum power dissipation for this device? how to calculate?
Regards,
Mark
Part Number: TS5A3153 Other Parts Discussed in Thread: TS5A3154 , SN74AXC2T245 Hi Sir,
Could you please tell me the Minimum limit frequency of the following parts?
Does it deal with a signal about 1Mpbs? I can not find related information in datasheet…
Part Number: TS5A3153 Team,
1. Do you confirm TS5A3153 can differentiate three states, i.e. NC, NO and Tri-state when the device is powered-up? 2. Do you confirm that when the switch in not powered-up COM pin is in High Impedance state? 3. When power…
Part Number: TS5A3153 E2E,
I'm looking for an analog switch (not sure whether SPDT can do the job) with the following specs:
They need to differentiate three different states, i.e. NC, NO and Three-State when the device is powered-up
When…
Part Number: TS5A3153 Other Parts Discussed in Thread: TMUX1119 e2e,
I'm currently testing TS5A3153 but coming across some issues.
Power Supply is 5V whilst EN and IN pins are driven by a 3.3V MCU.
According to the test results, they’re measuring…
Vineet,
but TS5A3153 gives maximum of 200mA current.
could you please send your requirements in details ..in word doc or pdf.
unable to see your figures.
Regards
Dinesh
Huang,
Yes, the TS5A3153 can pass a signal as long as it does not violate the voltage and current ratings of the device. The datasheet recommends not to exceed 5.5 V and 200mA through the signal path.
Thank you,
Adam
Other Parts Discussed in Thread: SN74LVC1G3157 , TS5A3153 , TS5A3159A Hello, in my circuit I need to choose between two signals to send to the output. One signal is a train of pulses (5V amplitude) coming from a comparator (open-collector output with…