Part Number: TS5A3159-EP Other Parts Discussed in Thread: TPS54260 Dear Team,
There is good new that we DIN the TPS54260 in customer's new project.
Customer have some questions as below, could you help to support it?
1. If we don't give V+ voltage,…
Part Number: TS5A3159 Hi Team,
Below is our test diagram.
Below is our test result. Output Vpp=0.86V, input Vpp=0.46V
Our input signal is 30MHz, Sine 2Vpp+DC 1V (Blue is OUT, Yellow is NC.) We think that the input attenuation is because that there is…
Part Number: TS5A3159 Hello,
We are using the device TS5A3159MDBVREP for one of our application.
For the digital control input pin no 6 of the device there is a transient with the following spec.
While switching from 0 to 5V at 3KHz rate,
Peak Overshoot…
Part Number: TS5A3160 Other Parts Discussed in Thread: TS5A3159A , TS5A3159 HI,
Could you please let me know the differences between TS5A3159 and TS5A3159A?
I found Ron of TS5A3159 is smaller than TS5A3159.
- Is the material of bonding wire same? - Are there…
Part Number: TS5A3159 Hi,
I have some questions for current parameter of TS5A3159DCKR, could you help to explain the meaning of below items?
1. II/OK
2. INO, ICOM (INC don’t need to define?)
3. ON-state peak switch current
4. IIK
5. Continuous…
Part Number: TS5A3159 Hi there,
I am interested to find out if the component can be used in Class 2 medical devices.
Also if it is possible, the operating relative humidity (RH) and operating pressure.
Thank you!
Part Number: TS5A3159 Customer would like to do the reliability review of this part. Could you offer the curve for ambient thermal versus output current? thanks.
Application: Encoder for Motor Drive
Part Number: TS5A3159 Hello,
in my low power design I use this circuit - standard high side switch - for blinking with high powerLED:
But in new generation of the product I need to save some space for additional communication circuit. Is it possible…
Hi Roy,
Thanks for your question. Your understanding is correct; the switch's internal architecture is a MOSFET. As typical with MOSFETs, lower supply voltages result in a higher internal resistance (ron). You can refer to the following table from the…
Part Number: TS5A3159-EP Hello,
What are the operating range and the absolute Max rating of TS5A3159-EP's junction temperature? They are not written in the data sheet, unfortunately.
Best regards, Shinichi Yokota