Part Number: TS5A3159-Q1 Dear TI Team,
my name is Igor Kuksin.
We are interesting to use this MUX in our application and I have one question.
It's mentioned in the datasheet, that in case the control input voltage level less than the supply voltage,…
Part Number: TS5A3159 Dear Team,
1.Is it necessary the NC and NO output pin have 50ohm during layout?
2.When Ch1(pin:6 IN) high, CH2 (pin:4 COM low), the CH3(pin:3 NC) didn't go low.
Is it because CH1 high just mean disconnect the COM to NC?
If I…
Part Number: TS5A3159-Q1 e2e,
For the analog input voltage, the TS5A3159-Q1 spec mentions max value is V + + 0.5V, but in note(3), it mentions that the output voltage rating may also be exceeded if the input and output clamp-current rating are observed…
Part Number: TS5A3160 Hi Sir,
Does TS5A3160DCKR has better performance than TS5A3159DCKR?
From Datasheet, TS5A3160DCKR ton/toff is faster and the price is relatively low.
The parameter I think will cause TS5A3159DCKR price higher than TS5A3160DCKR is…
Part Number: TS5A3159 Hi team,
I want to check if the NC pin is connected to COM pin when the VCC power is off.
If no, is there any analog switch that could achieve normal close when the power is off?
Best regards,
Shubiao
Part Number: TS5A3159 Other Parts Discussed in Thread: SN74LVC1G3157 , Dear Sir / Madam,
I am using hyperlynx for signal integrity simulations. I tried to use ibis file of TS5A3159 and get following errors.
* Warning : at line 108 in file ts5a3159.ibs…
Part Number: TS5A3159-Q1 Hi Team,
There is a customer that they want to use MUX to change the initial state of GPIO. Here is the block diagram for this application, they want a 34 channel device for this application.
Requirement parameter:
Vcom tolerance…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TS5A3159-EP We are looking to secure this exact same part (SN74LVC1G3157) but with a -55C to +70C operating temp. Is that something that is available?
Part Number: TS5A3159-Q1 Is its channel bidirectional? I assume it is based on MOSFETs and in that case it should be bidirectional but I could not find any reference to MOSFET in specification. The name of resistant parameter “Ron” tells nothing neither…
Part Number: TS5A3159-EP Other Parts Discussed in Thread: TS5A3159 Hi,
Is there an internal connection between the COM and GND pins on the subject PN?
Thank you,
HSG