Part Number: TS5A3160
Are there more details regarding the TS5A3160 Make or Break feature? Are there other parameters to be aware of when designing with this feature? Only the Tmbb is noted with little detail
Part Number: TS5A3160 Hi,
Regarding with connection of TS5A3160, I would like to know whether it can be used as both cases below? The reason I would like to ask is because, pin function description mention that NO (Pin 1), NC (Pin 3) and COM (Pin 4) are…
Part Number: TS5A3160 Hi,
Normally if VCC = 0V will put the device into shut down mode. But if VCC is still connected to 5V but GND is disconnected or left open, will it go into shut down mode as well?
Thanks.
- YY
Part Number: TS5A3160 Other Parts Discussed in Thread: TPL5110 , , CC3200 Hi,
I studied the document of Ts5a3160 switch. & TPL5110 Nano timer
I want connect nano timer ( www.ti.com/.../TPL5110 and micro controller( cc3200) through the switch(TS5A3160…
Part Number: TS5A3160 Other Parts Discussed in Thread: TINA-TI , , TS5A3159 Tool/software: TINA-TI or Spice Models Hi
Our customer is asking the way of investigation of charge injection for TS5A3160.
Can you share the TINA-TI simulation model to see the…
There are clamping diodes, i.e., there is a low-impedance connection to V DD . (The absolute maximum ratings forbid Sx/D voltages above V DD + 0.5 V.)
Use a 3:1 mux like the TS5A3359, or a 2:1 mux with powered-off protection like the TS5A3160 (see the I …
Other Parts Discussed in Thread: TS5A3160 , TS5A3159 Hi,
I'm using (or ~probably~ misusing :) a TS5A3160 to switch a 0 to 1.5V voltage to the base of two transistors:
I change the value on the 0-1.5V input and then switch the 3160. This is done at…
Dan,
The 0.1u capacitor is a decoupling cap used to reduce noise from circuit elements. The capacitor acts as a shunt to block off the noise. Using this external component is common practice on your supplies.
Regards,
Alex
Other Parts Discussed in Thread: TS5A3160 What is the difference between Break-Before-Make and Make-Before-Break?
Break-before-make (BBM) and Make-before-break (MBB) are two similar yet very different safety delay features that many analog switches / multiplexers…