Part Number: TPS22910A Other Parts Discussed in Thread: TIDA-00374 , TPL5110 , , TS5A3160 , TPS22916 Hi,
Referring to TIDA-00374 - looks like a good solution. Though since this a bit dated (May 2016) wondering if there are higher performing replacement/ upgraded…
Other Parts Discussed in Thread: TS5A3160 , TS5A3154 , TS5A23160 TI switches and multiplexers datasheets often include a plethora of different timing characteristics that help define exactly how each device will behave transiently under a certain set of…
Clemens Ladisch said:
V CC is the voltage at the V CC pin. The input voltage is the voltage at an input pin, i.e., CLR /A/B.
The CD74HC221 Operating Conditions do not allow a supply voltage lower than 2 V. (The Absolute Maximum Ratings just guarantee that…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TS5A3160 , Hello,
I'm looking for a power mux device for 1.8V and 3.3V with around 20mA. TI's power mux device basically doesn't support low voltage like 1.8V.
Is there any issue to…
Hi Jan,
What is the voltage level required for your application - I can see you are using 3.3V supply
You would also like to select a signal switch with before make feature to ensure you don't have issues connecting and disconnecting LED. Also, the…
Part Number: TPL5100 Other Parts Discussed in Thread: TS5A3160 , , TPL5110 , Hello,
I have problem with TPL5100. I'm designing device that needs to be powered on with 16 sec. intervals. I used TPL5100 to accomplish that with an analog switch (TS5A3160 to…
Part Number: CC2541 Other Parts Discussed in Thread: TS5A3160 , TPS62740 Hi,
Recently I have found out about following reference design to extend battery life.
www.ti.com/.../tida-00374
I have plan to use CC2541 in my application.
My questions are as…
I like to use external reference and internal reference simultaneously with user input from the program. So I like to use a switch between internal and external reference (1ohm max TS5A3160 from TI) Do you think this approach is suitable for the DAC8760 REFIN…
Other Parts Discussed in Thread: ADS1232 , TS5A3160 I'm doing a wireless weigh scale design using the ADS1232. Everything is working great but every once in a while, I experience a very large offset that doesn't seem to go away after battery replacement…