Hi Nicholas,
A couple other things, are you using a filter for the clock and/or input?
When you say clock is 19 dBm, is that at the sig gen or at the clock pin?
Regards,
Drew
Other Parts Discussed in Thread: ADS5409EVM Hello,
I have ADS5409EVM and TSW1400EVM. I want to capture data from TSW1400EVM by using Jetson Orin Nano (Linux). I can't find .so files for Linux in High-Speed Data Converter application. Where can I find…
Part Number: ADC3244EVM Hi,
We currently use 2 ADC3244 ADCs in a dual receiver architecture. We are experiencing an issue with receiver B not working during startup due to synchronization issues. Our start-up sequence is to rest all ADCs, set up each…
Part Number: AFE58JD48EVM Other Parts Discussed in Thread: AFE58JD48 Hello, everyone, and hello to all the members of Team Support: I have the following question. We are using the LVDS interface to connect our newly purchased AFE58JD48EVM to the TSW1400EVM…
Part Number: ADS5294EVM Other Parts Discussed in Thread: ADS5294 , Dear friends,
I am now designing ADS5294 + FPGA Board.
Cound you provide the FPGA HDL Code for TSW1400EVM (ADS5294 ...).
I have ADS5294EVM but, I did not use it.
My email address is yimidi…
Part Number: AFE5818EVM What could be causing significant fluctuations in the amplitude of ADC data over time when I connect AFE5818EVM to TSW1400EVM, and input a fixed amplitude 100mV, 1MHz sine signal to the input of AFE5818EVM using a signal generator…
Part Number: ADS5409EVM Hello,
I am working on a project that requires the rapid acquisition of analog data, and I may consider using an ADC evaluation board along with the associated data capture card. My application aims to retrieve data from a sensor…
Part Number: AFE5832LPEVM Other Parts Discussed in Thread: AFE5832EVM Hi, I can successfully set up and capture data from TSW1400EVM + AFE5832EVM using HSDC pro.
I now want to continuously collect data and observe real-time data through MATLAB (which may…
Part Number: AFE5818EVM
Hello :))
I'm using an AFE5818EVM to receive ultrasound signals along with a TSW1400EVM to capture and evaluate the data. This works very well. Thank you!
Now I would like to make use of a Raspberry Pi to automatically extract…
Hi Valerio,
Understood. I will check and get back.
A few questions in the meantime - how many averages do you want to do? If it is not a lot and you are only planning to do one time, you can record the files as detailed here ( https://e2e.ti.com/support…