Part Number: TUSB1210 Hello,
I'd like to know if the output capacitance of TUSB1210-Q1 really needs to be > 120uF in Host Mode. Why is it that high and under what circumstances can it be lowered?
In Device Mode it is 4.7uF - can that capacitance…
Other Parts Discussed in Thread: TUSB1210 , TUSB1210-Q1 Hi,
I have a question for VBUS of TUSB1210.
My customer don't use the VBUS.
Then, is it unnecessary to connect the VBUS pin?
On the datasheet p54, it is mentioned that "TUSB1210-Q1 does not strictly…
Part Number: TUSB1210 Hi Team,
I have customer that would use TSUB1210-Q1 with Jacinto6 6.
The TUSB1210 would be configured as input clock mode then. But the clock coming out from SOC is in tuning yet, not in good ppm quality.
So customer would like…
Part Number: DRA77P Other Parts Discussed in Thread: TPD12S015 , Tool/software: Linux Hi,
We intent to use the lcd1 interface for hdmi on our custom board.
The block diagram of the circuit is as follows,
We have made required changes in the pin mux and…
Q1: Is there any power sequencing required for TUSB1210?... In my current design, 3.3V (for VBAT) is enabled by GPIO from OMAP which is asserted only after 1.8V (for VDDIO) is powered. Can this create any issue with TUSB1210 and USB booting?
A1: Recommended…
Part Number: TUSB1210 Hello?
As the title, I would like to ask if there is a plan to release a 3.3V version for I/O level(ULPI) of the TUSB1210 product.
Please reply.