Hi, Can you please share your device tree overlay file, as well as full Linux terminal log. Also, can you please share log of below in Linux terminal. root@J7-evm:# ls -la /lib/firmware/ Best Regards, Sudheer
Tushar:
Now I am checking all of my Virtual Ubuntu USB serial ports before rerunning. I have run these commands before opening the serial ports within CCS:
sudo chmod a+rw /dev/ttyUSB0
sudo chmod a+rw /dev/ttyUSB1
but have not yet tried that on either…
Hi Roland,
When you consider this EVM is placed between the upstream facing micro-AB receptacle, and the downstream facing Type-C receptacle, these diodes are ok to have.
The diode in red allows VBUS to enter the VBUS switch from the UFP micro-AB receptacle…
Hi Brian,
TUSB322
TUSB320 is not pin-to-pin compatible with TUSB322.
The pin 3 & 4 are functionally different.
My customer needs DIR pin to evaluate the Type-C orientation detection; therefore, TUSB320 does not suffice.
HD3SS3202EVM
I checked the…
Hello Nick,
As per your suggestion link, we have added changes to our "k3-am62a7-sk.dts" file. We have added additional changes below, along with your suggested link.
Additional Changes: (Without below changes, DTB generation will fail.)
…
Part Number: AM6442 Follow-up Nick Saulnier 4/4/24
The execution of Booting Remote Cores — AM64x Academy
when one goes to running the echo stop, we have a failure ( from terminal screen looking at SD card)
root@am64xx-evm:/lib/firmware# echo stop…
Don't worry about the magnitude for now as yours setting might be different.
Please refer to user guide's schematic-
CH2 is Lead I = LA-RA CH3 is Lead II = LL-RA; supposed to be the largest vector(magnitude) There is no raw signal available/shown…
Other Parts Discussed in Thread: TUSB320-HA-EVM , TPS65987D , TPS65987DDJ , TPS65988DJ Hi
I'm looking for a USB PD controller that can:
- Connect to an Android tablet\phone as USB C
- Supply charging current to the Android tablet \phone
- Simultaneously…
Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320-HA-EVM , TUSB320 Hi
I have a TUSB320-HA-EVM development board, and I am trying to achieve the below:
- Connect an Android device, via USB C to the development board (in this case I’m using…