Part Number: TUSB320HAI Other Parts Discussed in Thread: TUSB320-HA-EVM , TUSB320 Hi
I have a TUSB320-HA-EVM development board, and I am trying to achieve the below:
- Connect an Android device, via USB C to the development board (in this case I’m using…
Hello Nick,
As per your suggestion link, we have added changes to our "k3-am62a7-sk.dts" file. We have added additional changes below, along with your suggested link.
Additional Changes: (Without below changes, DTB generation will fail.)
…
Erik Friedel said: 1. Do the Sitara MCU evaluation modules (EVM) and LaunchPads (LP) have any power requirements?
Sitara MCU LP/EVM’s require a 5V/3A supply. The USB Type-C Port Controller (TUSB320) only enables the device power tree's Power-on sequencing…
Hello Pablo,
For J7ES I expect the onchip trace to your R5 will work with any adaptor. The in the box adaptor with an EVM is not useful for off chip trace.
For off chip trace what is typically is a (LA-7992 or LA-7993 preprocessor) + (PowerTRACE-II/III…
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: SYSCONFIG Hello, I would like to control gpio on expansion connector("J3" exp_gpio0_36) of SK-AM62X EVM. I used sysconfig tool to generate dtsi file which is set as gpio. And, I add…
Hi Bin,
The SD cards as been tested on SK EVM using the SDK 6 image, that I have falsh on the SD card using bmaptool or dd. The boot was successfull. So I suppose the sd cards are working fine.
Here are the trace for the kingstone SDCARD:
U-Boot SPL…
Part Number: AM6442 Follow-up Nick Saulnier 4/4/24
The execution of Booting Remote Cores — AM64x Academy
when one goes to running the echo stop, we have a failure ( from terminal screen looking at SD card)
root@am64xx-evm:/lib/firmware# echo stop…
Hello Nick,
I reset everything, clean & build the dtb, and I finally got the access to ehrpwm4.
I also defined ehrpwm5.
Small question before closing this ticket: ehrpwm4 and ehrpwm5 are accessible through pwmchip0 and pwmchip2. Why is that? Should…
Part Number: TMS320F28386S Hi team,
I have questions about EOS flag use-case, I am referring TRM now. On "20.7 EOS and Interrupt Operation" mentions aout EOS pulse and register flag to use for interrupt event.
Q1. Is EOC flag set up on "20.15…
Hi,
If you want all 12 ECG leads to be acquired in analog, you will need two ADS1298(R) chips.
There are different options and approaches, Refer to EVM user guide 3.4.4.1 Wilson Central and Augmented Lead Registers and 4.6 Lead Derivation.
One could use…