Part Number: TVS1400 Hi Sir,
If I use TVS1400 at a power input. Then having a over voltage test like 22V power input for an hour.
Will the device burn down?
Thanks!
Part Number: TVS1400 Other Parts Discussed in Thread: TPD2E007 I am working on a design that includes the circuit as shown in the schematic here and am seeking guidance on both the choice and placement of TVS ICs which may include the TVS1400. The device…
Part Number: TVS1400 One of my customer requests variation data for these characteristics below.
Do you possibly have variation data with more than 1 lot and 100 devices are tested in each lot.
①VRWM (Reverse Stand-off Voltage)
②VBR (Break-down…
Part Number: TINA-TI Other Parts Discussed in Thread: TVS1400 Tool/software: TINA-TI or Spice Models Hi team,
I downloaded the TVS1400 spice model from http://www.ti.com/product/TVS1400/toolssoftware
But I can't add TVS1400 spice model into TINA9…
Part Number: XTR300 Other Parts Discussed in Thread: TVS1400 , TVS3300 , TVS0500 , TVS1401 Tool/software: Hi dear,
I would like to be sure which could be the best solution to protect XTR300, so, the power supply should be 24 V DC and -5 V DC, so I read…
Part Number: THVD1550 Other Parts Discussed in Thread: SN65176B , TVS1400 Tool/software: Hi,
What is the signal jitter of THVD1550 at a speed of 10Mbps and a cable length of 100 feet? Is it less than 20%?
According to the documentation, the cables…