Part Number: TX7316 Hi All,
TX7316 need specially Initialization Sequence in off-chip Beamforming mode besides power on reset?must it use SPI controlled?
Best Regards,
Charlie
Part Number: TX7316 Hi All,
TX7316 REGISTER ADDRESS table is really 00h~19H ,but SPI programing means A9~A0 D31~D0,
It is 8bit or 10 bit?
Best Regards,
Charlie
Part Number: TIDA-01371 Other Parts Discussed in Thread: TX7316EVM , TX7316 Dear support,
I have a question about import Altium design to Orcad, I know there is a feature of the Orcad that can import the Altium format, but it need the Altium design to be…
Part Number: TX7316EVM Other Parts Discussed in Thread: TX7316 Tool/software: Dear TI team,
Hello!
From the TX7316 datasheet, we learned that the TX7316 has 16 delay profiles in on-chip mode. To achieve continuous beam scanning, we need to switch between…
Part Number: AFE5851 Other Parts Discussed in Thread: TX7316 , TX7332 Am developing handheld ultrasound, Now I want to know if AFE5851 and TX7316 can works together/ interfaced together and
ALSO I want know if there is any reference designs to refer a…
Part Number: TX7316 We are looking at the TX7316 as a pulser/rx-switch for an ultrasonic front-end. During a market survey we noticed the STHV1600 which is more or less offering the same. Most likely TI has done "some" market research too and my questions…
Part Number: TX7316 Hi team
Good day, we got a problem:
we need to have the ability to drive an ultrasound probe in continuous mode and pulsed mode and then also be able to be able to read the reflected echoes.
TX7316 this part was unable to decipher…