Part Number: TX7332 I am a professor at Kangnam University in South Korea, leading a research laboratory focused on the development of ultrasound imaging systems. Our lab is planning to develop a small-form-factor ultrasound imaging system and is currently…
Part Number: TX7332
Hi,
As specified in the technical documentation, the TX7332ZBX is having two dies(die1 and die2). Each of two dies (die 1 and die 2) has its own register map. Registers referencing channels 1-16 are associated with die 1, and registers…
Part Number: TX7332 Hello, thank you very much for your reply. When using the channel delay function of the TX7332, my configuration is as shown in the picture. When I set the delay to 1200, everything works fine. However, when I configure the delay to…
Part Number: TX7332 Other Parts Discussed in Thread: AFE5832LP Hello E2E Experts,
I have already bought the AFE5832LP and TX7332 cores.
Now I faced several problems when I using them.
Please refer to the attached files.
issue.docx
300delay.docx…
Part Number: TX7332 Dear Team,
Please provide the complete datasheet of TX7332ZBX including schematic symbol name and pinout details as well as the footprint data. For adding the component to our centralized library we need these information. Kindly…
Part Number: TX7332 Tool/software: I have 2 tx7332 use on board. The schematic as sane as the reference design. The system run for 13 minutes and one of the tx7332 is burned
what can be the causes for this ?
Part Number: TX7332 Other Parts Discussed in Thread: TX73H32 Tool/software: Hi,
As specified in the technical documentation, the TX7332 can store up to 16 delay profiles. However, when performing ultrasound beamforming, I require at least 128 delay…
Part Number: TX7332 Hi Team,
Posting on behalf of our customer.
If I wanted to drive a larger load (e.g., a probe with a shielded cable of length 1-3m commonly used in ultrasound imaging), would I need to upgrade both the TX7332 chips and the power…
Part Number: AFE5816 Other Parts Discussed in Thread: TX7332 We are currently engaged in the software design for Ultrasonic Non-Destructive Testing Equipment using the TX7332 and AFE5816 chips. Our development platform is based on the Zynq-7000 series…
Part Number: TX7332 Tool/software: When a single AFE is wired to two TX7332 (e.g. Ch0 on the AFE connected to Ch0 on TX1 and ch0 on TX2), how do I get a signal only from the one TX at a time? I do not understand how the TR switch should operate. Either…