Hi Kamlesh,
If you disconnect UC1708 and 5K resistor , are you still seeing pulses out of UC1524 at zero duty cycle.
Zero duty cycle implies there are no output pulses. Zero duty cycle relates to where the E/A output crosses the ramp. As this…
Part Number: TPS7H5005-SEP Other Parts Discussed in Thread: UC1708-SP I am trying to build a push pull isolated DC/DC converter. Vin 26-34V, Vout 28V, Iout 10A. I am not opposed to using two converters to share the load using the Sync pin. My use case…
Aaron, thank you for the response. Pin-to-pin compatibility with ENABLE input floating is neat, but my main concern with UCC27323 and UCC27423 is the max Vdd of 15 V while the discontinued UC1711 supported Vdd = 35 V. What about PNs UCC27624 or 5962-0051401VPA…
Part Number: UC1823A Other Parts Discussed in Thread: UC1708 I am reviewing an old motor control design which we may have an opportunity to update. The power supply currently uses an UC1823A PWM controller and UC1708 dual FET driver. Must meet -55 to…
Part Number: UC1823A Hello - I am reviewing an old motor control design which we may have an opportunity to update. The power supply currently uses an UC1823A PWM controller and UC1708 dual FET driver. Must meet -55 to 125C military temp range. Is there anything…
Other Parts Discussed in Thread: MKT-WG16A-MS , MKT-WG10A-MS , SN0020HKH , SN0010HKU , TPS7H1111-SP , TPS7H6003-SP , SN00020FK Looking for mechanical package samples for trim and form setup
Answer:
For our Space Power Ceramic QMLV qualified portfolio of devices…