Part Number: UC3906
Hello
I'm repairing a laser controller in my laboratory.
but the laser controller is over 20 years old and is not supported by the manufacturer...
so I disassemble and repair it myself, looking at the circuit board.
Currently, I…
Part Number: UC3906 Other Parts Discussed in Thread: BQ24450 , , UC2906
Hi team,
This is Xiaoying, my customer is utilizing BQ24450 but recently they are facing with shortage issue.
We find that UC3906 might be a good alternative as it is pin-to-pin with…
Part Number: UC3906 Hi there
I used the uc3906 to charge the 24v battery. Supply voltage for uc3906 from 39V to 40V, can Uc3906 work 24/24 continuously?
Thanks for your help
Truong Nguyen
Part Number: UC3906 Other Parts Discussed in Thread: BQ24450 , BQ24650 Hi,
UC3906 is not recommended to the customer at present. Is there any new plan to replace TI? Is it a P2P solution
Best Regards
Leon
文晔集团
广东省深圳市南山区高新中三道 9 号环球数码大厦 12 楼
Mobile:(86)159 8985…
Part Number: UC3906 I working on Float *** boost charger, Using IC UC3906. Battery rating 24V, 150Ah, at 10Hr charging rate. 1+1 redundancy is required, and each should share load. Problem i am facing how to operate two UC3906 in parallel with load sharing…
Hi Raheem Thank you so much for your response it is very much appreciated . The Value of R2 is as in the Schematic 0.15Ω 5 watt resistor .
I have tried to use the Design Procedure on page 5 of UC3906 Datasheet . but i am totally lost . is it possible…
Part Number: UC3906 I need 48 V to power a 5KW inverter of my solar system,I had design a 12V charger with this ic successfully,now I wonder it can charge 4 SLA battery in series?
Other Parts Discussed in Thread: UC3906 , BQ24450 Hi!
I´m building a 3A 12V battery charger, using the UC3906.
If I understood the datasheets correctly, with Imax = 3 A, Ioct needs to be about 0.3 A in order for the circuit change from overcharge…