Part Number: UCC12050 Hi,
My customer is considering using UCC12050.
They would like to know if UCC12050 can output 550mW surely.
However, I can not find specifications regarding output power.
Is the maximum output power guaranteed?
Best Regards,
Kur…
Part Number: UCC12050 Hi Team,
Hope you are all doing well. I'm reaching out to you because I want your advice regarding the "galvanic isolation capacity" for UCC12050.
I'm looking forward for your response. Thank you in advance for the support…
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 , UCC12051-Q1 , Hello,
We would like to check whether the SYNC input pin can be driven with an external 3.3V clock signal, which seems feasible based on the datasheet.
Could you please confirm…
Hi Jared,
Thanks for the photograph. The resolution is high enough that I was able to zoom in and examine it very closely.
If I traced it correctly, and if you are using 10-uF SMD tantalum capacitors on each output, then I think C10, C14, C18 and C22…
Part Number: UCC12050 Other Parts Discussed in Thread: UCC12040 Regarding Synchronization of the part. Is it NECESSARY to use an external clock, or can you simply connect the SYNC pin of one UCC12050 to the SYNC pin of another UCC12050? It is not clear…
Part Number: UCC12050 Other Parts Discussed in Thread: DCPA10515D , Hi Team,
Good day, we received a query from customer and for me to not miss any information, I'll copy the query below. "
I'm looking for a small volume DC DC converter (<5W) with…
Part Number: UCC12050 Hello experts,
I would like to get a certificate from a certification body for CTI.
I asked UL about insulation distances and was told that they would not accept CTI ≥ 600 without a certification from a certifying body regarding…