Part Number: UCC14130-Q1 Tool/software: I have a design that uses the UCC14130-Q1 part in the single output configuration to generate an 18V nominal output from a 15V regulated input (configured like figure 12-2 of the datasheet). My design has 20uF…
Part Number: UCC14130-Q1 Tool/software: I'm using several of these DC/DC modules in my design. The other configurations appear to be working fine but I have a startup issue with one configuration. This configuration is providing 15V (40mA) and 5V…
Part Number: UCC14130-Q1 Tool/software: Hi team,
I saw below User's guide.
https://www.ti.com/lit/ug/sluubd5d/sluubd5d.pdf?ts=1735033989453#page=12 (stitch capacitor)
https://www.ti.com/lit/ug/sluucj2c/sluucj2c.pdf?ts=1735034622153#page=28 (no layout…
Part Number: UCC14130-Q1 Tool/software: I'd like some help understanding the effect of a too-small RLIM resistor on the COM-VEE regulation and how to avoid this.
My goal is to choose RLIM such that a variable load can be connected across VDD-COM which…
Part Number: UCC14130-Q1 Tool/software: We're planning to use the DCDC converter IC, UCC14130-Q1, and bullet 7 on page 48 of the datasheet recommends no copper under the part. I understand this for creepage, but we will likely have copper on internal…
Part Number: UCC14130-Q1
Tool/software:
I have selected the UCC14130QDWNRQ1 as a DC-DC isolated power supply to isolate a 12V power source. I intend to use it for a single output. However, I could not find specific guidance for this use case in the datasheet…
Part Number: UCC14130-Q1 Other Parts Discussed in Thread: UCC14341-Q1 , UCC14340-Q1
Tool/software:
Dear TI,
I am designing a system that requires isolated 12V, -12V, and 3.3V outputs from a regulated 12V input supply. The isolated power will be used to…
Part Number: UCC14130-Q1 Is a PSPICE model available for the UCC14130-Q1? I have PSPICE A/D 17.4. I have a motor drive simulation and would like to add the UCC14130 to power the MOSFET drivers.
Thanks,
David Jarvis
L-3 Harris / Coleman Aerospace.
Part Number: LM25183 Other Parts Discussed in Thread: UCC14130-Q1 , LM5180-Q1 Tool/software: Hi,
We are considering a simple isolated power supply configuration for a new application.
①Vin +12V, Vout +5V, Iout 500mA ②Vin +12V, Vout +24V, Iout 300mA
As far…
Part Number: UCC12040 Other Parts Discussed in Thread: UCC14131EVM-070 , UCC14130-Q1 Tool/software: Hello,
I need to develop power supply of the following conditions:
1. Isolated
2. 12V to 12V
3. Max output power 3W
4. At no output load, this power supply…