Part Number: UCC21530-Q1 Other Parts Discussed in Thread: UCC21530 Tool/software: Hello, I am using the UCC21530 gate driver to drive Half bridge and during lightneing pulse test, the gate driver is damaged (only one / 3, always the same which is damaged…
Part Number: UCC21530 Other Parts Discussed in Thread: UCC21551-Q1 , UCC21330 , UCC21551 Tool/software: Hello, We are looking for a robust and reliable isolated and/or non-isolated half bridge gate driver for a 120V 6kW PMSM motor driver ; 1- We are wondering…
Part Number: UCC21530 Other Parts Discussed in Thread: TIDA-00366 , I was referring to TIDA-00366 document. I assume that the DC voltage generated would be in the order of 400V if the input supply is 230V,50Hz. Whether the DC voltage is sufficient for the…
Part Number: UCC21530 Other Parts Discussed in Thread: ALLIGATOR Hi
We used four boards of this model. After the computer test, one of the boards was abnormal and did not respond, and there was no output after the PWM input was given. Could you please…
Part Number: TIDA-00366 Hello,
I have a designed a 12KW 3 phase motor inverter using many of the hardware and design circuits from TIDA-00366. The design can be tailored for Scalar, Sensored or Sensorless control by including or emitting components based…
Part Number: UCC21530-Q1 In my current application a three phase 2 level inverter is used to control a PMSM.
I'm using UCC21530-Q1 to drive SIC mosfet. Swtiching frequency is 20 kHz and switching speed in the range of 50 ns.
min and max duty cycle…
Part Number: UCC21530-Q1 Other Parts Discussed in Thread: UCC21530 Regarding boostrap capacitor, what are recommandations from TI when we have no switching commutation for a long period of time (>30s).
Shall we start we a precharge of boost strap capacitor…