Part Number: UCC21530 Other Parts Discussed in Thread: UCC21551 Hello :
inport ucc21530 PSPICE model on TINA,missing syntax element line : #65
how to fix it?
Best Regards
Part Number: UCC21551-Q1 Other Parts Discussed in Thread: UCC21331-Q1 , UCC21530-Q1 Hi e2e:
Could you please provide the information about dv/dt of the VDD of UCC21551-Q1 and UCC21331-Q1?
Part Number: UCC21530 The UCC21530 datasheet lists a VDD to VSS UVLO for the UCC21530-Q1, but does not list anything for the UCC21530. Does the UCC21530 have a VDD to VSS UVLO? Or is the UVLO only applicable to the -Q1 parts?
Part Number: UCC21530 Other Parts Discussed in Thread: TIDA-01605 , UCC21520 Hi,
We have a 3 phase inverter, built with SiC MOSFETS being driven from UCC21530 in a setup similar to TIDA-01605.
During some test cases where we had our controller's PI loop…
Part Number: UCC21530 Hi Team,
Can you please help answer the question below?
Regarding the output stage in Section 8.3.4 of the data sheet,
When the circuit is designed according to the connection shown in its schematic diagram, the signal passing…
Part Number: UCC21530 Hi,
I drive one Si MOSFET. There is no power transfer on it and no drain voltage on it.
I attached test circuit diagram and Vgs waveforms. The Vgs of MOSFET isn't close to zero volt. It is 1,28V and its upper level is 13,95V.…
Part Number: UCC21530 Hi, hope this finds you well.
I am testing the gate driver UCC21530QDWKQ1 and encourter some problems. The output Vgs ls as the following picture shown: for a period of time, Vgs is alway in high, and the other time, Vgs is normal. But…
Part Number: UCC21530-Q1 Hi Team,
Could UCC21530-Q1 operate as 100% duty cycle?
Will both high side and low side need to support 100% duty cycle?
Could you give more details this 100% duty cycle operation?
Will both high side and low side have its…