Part Number: UCC21736-Q1 Hi expert,
I want to use the UCC21736 to drive 3 SIC MOSFETs connected in parallel, as shown in the figure below, how to implement External Active Miller Clamp function?
Part Number: UCC21736-Q1 Dear Team,
I've tried to simulate the circuit in LTspice using UCC21736-Q1 unencrypted spice model. But I'm getting the following error (U1:e_abm85: Unknown circuit node: "u1:u1_asc_inv" requested in behavioral source)…
Part Number: UCC21736-Q1 Other Parts Discussed in Thread: LMG1210 , LMG1205HBEVM , UCC21540A , LMG1205 , UCC21540 Hi,
I have an application where I need to drive a Silicon MOSFET (Part number: SISS08DN-T1-GE3; Datasheet: https://www.vishay.com/docs/76780…
Part Number: UCC21736-Q1 When using the miller clamp function of UCC21736-Q1,whether an external MOSFET is needed,or I can refer to this figure directly
Part Number: UCC21736-Q1 Other Parts Discussed in Thread: UCC21732
Hello,
we have designed a gate driver with the UCC21736 IC, and it seems that the output does not want to switch when the VEE is at the same potential as the COM on the output.
The part…
Part Number: UCC21736-Q1 Hello, i have a question regarding the OC protection on UCC2173x family. If i use SiC device without SenseFet Pin (Source Sense pin), which is the best method to implement current scale down? OC pin requires 0.7V to trigger, for…
Part Number: UCC21736-Q1 Hello,
it was mentioned in other threads that there are datasheet inconsistencies regarding the gate driver UCC21736-Q1.
I would like to know if switching is possible with a Vee-Vcom of 0V?
In the datasheet (from APRIL 2020–REVISED…
Part Number: UCC21736-Q1
Dear TI
I test A UCC21736 Reference Circuit. then Reference information , R28 Resistor Value is different in Circuit vs in Part list.
Why?
Best Regards,
Choi
Part Number: UCC21732-Q1 Other Parts Discussed in Thread: UCC21739-Q1 , UCC21710-Q1 , UCC21750 , UCC21736-Q1
Hello everyone,
I need a high current gate driver and all of these drivers meet my needs. But I need to pick one or two. I went through the datasheets…