Part Number: UCC24612 Hello,
I use UCC24612-2 in LLC secondary side.
The application is a 48V-30A power supply with 4 mOhms MOSFET.
Here is the thing : I have a value of VREF well regulated to 9.5V, with only a small HF ripple of 150mV.
So I expect…
Part Number: UCC24612 Hi team,
Does the UCC24612 include internal negative-voltage protection, such as a Schottky diode, between the VD and VS pins? If so, is an external protection diode required?
Best Regards,
Ryu.
Part Number: UCC24612 Hi,
I am interested in using the UCC24612 as a synchronous rectifier controller for a CLLLC converter with 325V output voltage.
Per the datasheet, the drain voltage sense pin is rated to 230V. I read through older forum posts…
Part Number: UCC24612 Hello guys,
One of my customers is considering using UCC24612.
At this moment, they have the following questions. Could you please give me your reply?
Q1. Can UCC24612 be used for like the attached circuit?
Q2. If there is…
Part Number: UCC24612 Other Parts Discussed in Thread: UCC24610 , Tool/software: Hello team,
can you share with me a spice model for:UCC24610 and UCC24612
thanks
Mat
Part Number: UCC24612 Other Parts Discussed in Thread: UCC24624 , PMP20878 Hello TI Experts,
I am working on a 250 W Active Clamp Forward converter and would appreciate your review and guidance on my design.
Project details:
Topology: Active…
Part Number: UCC24612
SMPS Wattage
Annual Qty
Part required
10 to 500W
40-50K
PWM controller
150 to 500W
25-30K
PWM, PFC, SR
We require FAE support for above mentined requirement…
Part Number: UCC24612 Hi team,
Gate resistance in the EVM schematic is 2.2 ohm. VGH is 9.4 V(typ).
Maximum source current is 1A and it seems smaller than 9.4V/2.2ohm. Is this no problem?
Best regards, Goto
Part Number: UCC24612 Hi team, Is it possible for the proportional gate drive function to turn ON/OFF due to time constraints when VDS changes near the threshold? I'd like to know how many seconds the threshold must be exceeded for the proportional gate…