Hello R.Rajesh,
Unfortunately for this design, Gerber files are no longer available.
The Schematic BOM and layer plots are illustrated in the User's Guide on the EVM page for this design.
The EVM is still orderable as well: http://www.ti.com/tool/ucc25600evm…
Other Parts Discussed in Thread: UCC24610 , UCC25600EVM , PMP8920 Hello-
We are developing the power front-end which includes 2 converters. The 1 st being the PFC section and the 2 nd is the isolation converter which may be the LLC resonant Half-Bridge. The…
Hi Mahesh, I guess the first question is whether your application needs PFC? For this kind of power level, a Boost PFC followed by and LLC is the most commonly used topology at the moment. The UCC25600 contoller could be used for the LLC, you can have…
Other Parts Discussed in Thread: UCC25600EVM , UCC25600 Hi,
I need to design a power supply of about 420W and I want to use as start point the evaluation board based on the reference design EVM note "UCC25600EVM" -sluu361.pdf.
I am not able to…
Other Parts Discussed in Thread: UCC25600 , UCC25600EVM HI
I have UCC25600 300W EVM with me and I trying to modify this eval board for my requirement, just want to understand whether the layout constraints in the Eval board will meet my new requirements…
Other Parts Discussed in Thread: UCC28070 , UCC28070EVM , UCC25600EVM Hi,
I am trying to power on the UCC28070 300-W Interleaved PFC EVM. I followed the below steps and i did not get 390V at output. Am i missing anything here? my setup is 230VAC from…
Hi, Dieter,
The group has released the design, and you can buy one, but I don't see the gerber files.
http://www.ti.com/tool/ucc25600evm-644#Technical Documents
-d2
Loc,
I designed a 300W offline LLC half bridge a few year ago. I used the UC2860. The UCC25600 is a good chip to use as well.
I used the Unitrode app note,U122, "A New Family of Integrated Circuits Controls Resonant Mode Power Converters" by Larry Wofford…
Other Parts Discussed in Thread: UCC28061EVM , UCC25600EVM Hi,
The customer is now surveying a 250W adapter power and it can meet Energy Start 2.0
Application: Adapter power for medical/industry
I/P:90Vac~264Vac; O/P:12V
SPEC: Follow Energy Start 2.0 (Especilly…