Hello,
Q1: Ipolarity comparator has 30.7 mV of hysteresis.
Q2. The open loop gain of Op Ams is generally 60-80 dB. The gain with feedback for Ipolarity Comparator pin can be generated by algebraically solving following equation for ( Ipolarity Comparator…
Part Number: UCC256302 Hello,
Does the UCC256302 operate the power switches at a constant frequency, with variable duty cycle or a constant duty cycle, varying switching frequency around resonance?
Please let me know.
Thanks
Hi
1. I didn't get the feedback too.
2. your questions are not showing at datasheet , so it is too confidential to share.
3. for your waveform , you should increase the Vcc voltage around 15V , and you need to keep RVcc stable at 13V , otherwise it…
Hi ACGUY,
do you send the waveform to Yunsheng by mail?
he is leaved TI , so please loop me into mail , and we can discuss at mail and close this post.
thanks
adamlin@ti.com
Part Number: UCC256302 Other Parts Discussed in Thread: UCC256402 Hi Team,
There is a description on the data sheet, "If there is no slew detected, IPolarity signal is used. The next gate will be turned on at the next IPolarity flip event."
…
Part Number: UCC256302 Hello E2E,
In the simplified schematic of the datasheet, Cr(resonant cap) is one. Hewever, the schematic of the EVM has two resonant caps on high-side and low-side. 1: Is it TI's original method? 2: Please let me know the usefulness…
Part Number: UCC256302 Other Parts Discussed in Thread: UCC256402 Hi Team,
I sometimes miss dV / dt detection for automatic dead time adjustment at room temperature.
Is there any information that high temperature and low temperature are more severe? …
Part Number: UCC256302 Other Parts Discussed in Thread: UCC256402 Hello E2E,
On the p32 of datasheet, that say "Fault conditions encountered by UCC256302 will cause operation to stop". Is this "operation to stop" latched stop?
Regartds…
Part Number: UCC256302 Other Parts Discussed in Thread: TMS320F280025C , Hi,
I am designing an LLC converter for a customer. The output is variable from 48V-400V. This is achieved by swapping LLC resonant tank and secondary side components for higher voltage…
Part Number: UCC256302 Other Parts Discussed in Thread: UCC256402 Hello,
I have a question about the detectable slew rate of dVHS / dt. The slew rate recognizes that 1V / ns ~ 50V / ns must be detected when Vds< 50V. ①Is there a minimum time required…