Part Number: UCC2583 私はUCC2583を使用しています。出力が短絡すると、電流はCSピンによって制限されます。また、出力が短絡している間は、電流制限が繰り返されます。電流が制限されている場合、UCC2583をすぐに停止するにはどうすればよいですか?%MCEPASTEBIN%(パーセント・マケペースト・ビン)
Part Number: UCC2583 Hi Team,
My customers have rated UCC2583.
They would like to synchronize the SYNC output with the RAMP output, but not.
It operates at SYNC 130kHz and RAMP 100kHz.
Why not sync?
SS terminal is connected to VREF terminal…
Hello Prajakta, There are 2 ways to create the second output. 1. Secondary Side Post Regulator. SSPR http://www.ti.com/product/LM25115A http://www.ti.com/product/UCC2583
This is a buck topology more suited for designs that have a main loop controlled…