Hey Karthik,
1. You are correct. You cannot use the UCC27212A-Q1 with a 280V bus voltage. For a driver that can withstand a 300V bus and does not have interlock, the only thing in our portfolio is the UCC27714. It is not automotive qualified as you have…
Part Number: SM72295 Other Parts Discussed in Thread: UCC27301A-Q1 , UCC27289 , UCC27211A , UCC27201A , UCC27282 , UCC27284 , UCC27311A-Q1 , BQ2031
Is it possible to use this part in a single half-bridge configuration i.e. the 'A' side to implement a low-cost…
Hey Peter,
Thanks for your question regarding UCC27282.
For your application, it seems that a good reference design for this is the Automotive 1-kW 48-V BLDC Motor Drive Reference Design .
This is a 1-kW system and utilizes the UCC27201A-Q1 as opposed…
Part Number: UCC27282 Other Parts Discussed in Thread: LM5101C , UCC27211 , UCC27211A , LM5101A , UCC27288 , UCC27301A-Q1 Dear all,
Background:
My customer now are designing a 4 switched Buck-Boost converter. And they are using UCC27282 as the gate driver…
Part Number: UCC27282-Q1 Other Parts Discussed in Thread: UCC27282 Hi team,
The following figure is my design. The function I want to achieve is to output high-voltage periodic square wave.
The supply is 12V,input is the 5V@11Khz,output is 90V,Theoretically…
Part Number: UCC27284-Q1 Other Parts Discussed in Thread: UCC27284 , UCC27282 , UCC27201 Hello
when adding the UCC27284 transient model PSPice mentioned: not a valid library file.
can you help?
thanks
Martin
Hi Jonathan,
I'll start with a basic question and answer. The UCC27282-Q1 version is the same IC design but qualification testing is more extensive on the automotive grade devices.
Can you provide a schematic of the power train and driver IC to be…
Part Number: UCC27284-Q1 Other Parts Discussed in Thread: UCC27282-Q1 , Hi team,
For which application without interlock is UCC27284-Q1? UCC27282-Q1 is with interlock and looks this function is needed for general half bridge application. If you have any…
Hi Sherry,
Thank you for reaching out on E2E!
The test conditions on the datasheet seem to be missing extra rows for the test conditions. I have attached to table below with the proper test conditions below.
When IN = Low and EN = Low, the Idd is 150…