Part Number: UCC27424-Q1 Hi team,
Is thermal pad of HVSSOP package separated/floating from any pins (1~8)? UCC27424QDGNRQ1 is a device with HVSSOP package.
Regards, Ochi
Part Number: UCC27424-Q1 Other Parts Discussed in Thread: UCC27424 Hi,
UCC27424-Q1:
1. is there pull-down resistor with INA and INB? what's the value?
2. is there ESD diode in output stage? what's the current ability of ESD diode in output stage?…
Other Parts Discussed in Thread: UCC27624 , UCC27424 Hi...
We are planning to use UCC27444QDGNRQ1 (uc27444-Q1) in our application.
Kindly share with me the PSPice for TI model of the part mentioned above.
Thanks in advance.
Best Regards,
Prahaladh S …
Part Number: UCC27424-Q1 Hi support team,
My customer wishes to know what is the min value for the rise time and fall time of UCC27424-Q1. The datasheet only specify the typical and maximum value, could you please check on this?
Thank you.
Best Regards…
Part Number: UCC27424-Q1 Hi,
For the UCC27424-Q1, do the OUT pins have ESD protection on them? This was not clear to me from reading the datasheet.
Best regards, Ross
Part Number: UCC27424 Hello guys,
One of my customers uses UCC27424DR for their mass production.
They found that the device datasheet was updated from version SLUS545E to SLUS545F recently . At this moment, they have the following questions about the new…
Hi Nick,
the support for this product is very limited at this time.
The following additional existing documentation can still be downloaded:
Resonant Trimming Sequence
TMS3705 Range Extender Power Solution Using UCC27424-Q1
TMS3705 Passive Antenna So…
Other Parts Discussed in Thread: UCC27524A-Q1 , UCC27424 , UCC27424-Q1 Hello,
Customer needs propagation delay matching data between 2 channels.
UCC27524A-Q1 has specification “ Delay matching between 2 channels: 1ns typ, 4ns max” and UCC27424 has…
Other Parts Discussed in Thread: TMS3705 Hello Guys,
I work with TMS3705 for many time. Now I´m making a solution using NEOSID antenna. I´m using 400uH, Q=60 - partnumber: 88 8049 66
www.neosid.de/fileadmin/user_upload/download/NEOTAG-Produktinfo…