Part Number: UCC27518 Other Parts Discussed in Thread: UCC27517 , UCC27519 , There are missing subcircuits in this model.
The UCC27517 model is fine but has different inputs.
Thanks for help
Dietmar
Part Number: UCC27518 Other Parts Discussed in Thread: UCC27519
Team,
Note: it is known that the IN pin is CMOS level and the EN pin TTL level
-In order to use UCC27518 as alternative to UCC27519: Can the enable pin be used as a non-inverting input and…
Other Parts Discussed in Thread: UCC27518 Hi,
I received the question from my customer about terminal capacitance of UCC27518.
Could you tell me the capacitance of +IN terminal and EN terminal?
Thanks and Regards,
Kuramochi
Part Number: UCC27519 Other Parts Discussed in Thread: UCC27518 Dear TI experts, The following is the circuit on our new product, please help to review whether there is any problem with the design, thank you!
The gate driver's output impedance is much lower, so it is easier to control the effective impedance with a series resistor.
Both the UCC27517 and UCC27518 have three models. (See the "Design tools & simulation" tab on the web site.)…
Part Number: UCC27519A-Q1 Other Parts Discussed in Thread: UCC27518 , LMG1020 Looking for a drop in replacement for this piece as it is out of stock pretty much everywhere - mainly looking for something that I can source easily now with the same UVLO.
…
The TLV1805 has a typical short-circuit current of 100 mA, but as far as I know, there are no comparators that can reasonably drive such a high output current through a load.
Does the input signal have proper logic levels (at least 3.3 V)? In that case…
A list of schematic review templates for many of our devices are available below! These templates are meant to be used in conjunction with our datasheets to help designers review their schematics.
UCC27516 and UCC27517 Schematic Review Template
UCC27511…
Part Number: CSD19532KTT Other Parts Discussed in Thread: LM5114 , UCC27518 Hello TI Community
I am designing Battery Management System 100V/100A and planning to use MOSFET CSD19532KTT. I will mount the Mosfets on the PCB and Mosfets will be placed in Low…
Hi Ville,
The UVLO circuitry may not put the device into a low-power state. For example, it pulls the gate of the mosfet low, so this will result in some current consumption.
If you need an enable pin, I suggest you look at one of our products that…