Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: UCC27519 Hi,
I will use the UCC27519 to drive a piezo. The application is a time of flight measurement in order to determine the velocity of sound in liquids. In our case the jitter determine the accuracy of the measurement…
Other Parts Discussed in Thread: UCC27519 HI Expert,
Below measuremnt is coming from the UCC27519 IN pin.
The negative voltage level is over the min rating of the spec defined.
Since this duration is very narrow,pls help to advice whether any risk had. …
Part Number: UCC27518 Other Parts Discussed in Thread: UCC27517 , UCC27519 , There are missing subcircuits in this model.
The UCC27517 model is fine but has different inputs.
Thanks for help
Dietmar
Chong,
Thanks for reaching out!
------
Regarding the simulation model for UCC27519A-Q1, the models are available for the "standard" part, the UCC27519. You can find them on the UCC27519 product page.
The major difference between them is, the…
Hi Woon,
Thanks for reaching out!
-------
Our LMG1020 can provide 0.4 ns typical rise and fall times (100pF load), BUT is limited to a 5V VDD... (If you can deal with the 5V limitation, this is the best choice)
It also has our smallest propagation delay…
Part Number: INA195 Other Parts Discussed in Thread: UCC27519 , LMV431 , , TIDA-01590 , INA260 I am designing some sort of a low current e-Fuse (10mA threshold) at 600Vdc application. We would like to provide a "test port TP" for service personnel to check…
A list of schematic review templates for many of our devices are available below! These templates are meant to be used in conjunction with our datasheets to help designers review their schematics.
UCC27516 and UCC27517 Schematic Review Template
UCC27511…
Hi Varunesh,
Please find attached a simulation based on your description of the input signal and schematic.
Notice that I am using UCC27519 instead of UCC27527. Reason for that is the similar input/output structures and input thresholds.
The simulation…
Part Number: UCC256303 Other Parts Discussed in Thread: UCC27519 Hi,
I hope now the pictures are added.
I am developing an insulated DC-DC converter using UCC256303 QR controller.
Two UCC27519 are inserted between the UCC256303 high side gate and low…
Part Number: UCC256303 Other Parts Discussed in Thread: UCC27519 Hi,
I am developing an insulated DC-DC converter using UCC256303 QR controller.
Two UCC27519 are inserted between the UCC256303 high side gate and low side gate wires and the MOSFET, as…