Part Number: UCC27531 Other Parts Discussed in Thread: UCC27710 Tool/software: Hello,
Could you please share the dv/dt immunity of the UCC27531 (Volt / nano-sec)?
Thank you, Keith
Part Number: UCC27531 Tool/software: Hello,
Just want to confirm that the output of the UCC27531DR cannot go high impedance? Even in an over-temperature condition, or other fault condition?
The "DR" version does not have the OUTH and OUTL pins.…
Part Number: UCC27531 Tool/software: What is maximum continuous current we can draw from the OUTH pin and continuous sink current rating of OUTL pin of UCC27531, I want to use this to drive a load which is consuming 50mA of current from 28V continuously…
Part Number: UCC27531-Q1 Tool/software: On the Functional Safety Information UCC27531-Q1 Functional Safety FIT Rate, FMD, and Pin FMA document: Page 4 there is a duplication, is this a typo, and what is supposed to be in its place?
Part Number: UCC27531 Tool/software: Hi Forum Members
Can anyone assist with why we have catastrophic failure of the UCC27531 on turn on - Q3 not switched on? Vcc is 16-24Vdc, so well within specification. When I lift the EN pin on the proto PCBs, the…
Part Number: UCC27531-Q1 Other Parts Discussed in Thread: UCC27624 , UCC27531 Tool/software: I am planning to use the UCC27531-Q1 2.5-A and 5-A, 35V MAX VDD FET and IGBT Single-Gate Driver to drive the SCT2H12NZ 1700V, 3.7A, THD, Silicon-Carbide (SiC…
Part Number: UCC27531 Hi All
In the drive circuit below it would appear that pin-2 of UCC27531 would be at 31V (13V + 18V) with respect to its GND pin-4 when the transistor within the optocoupler is off thus exceeding the absolute maximum rating of 27V…