Other Parts Discussed in Thread: UCC27710 , UCC27712 , UCC27714 Tool/software:
Kind regards.
The image says interlock and deadtime. When you search the data sheet, deadtime isn't listed.
Part Number: UCC27714 Other Parts Discussed in Thread: UCC21710 , ISO7740 Tool/software: Hello TI,
We're using the UCC27714 to drive an HBridge with a power transformer. I'm seeing a large spike due to the Miller capacitor when the high-side transistor…
Part Number: UCC27714 Other Parts Discussed in Thread: ISO6741 , ISO6441 Dear TI team,
Please find the attached document for the review. I have added some questions in the document request you to please provided the response.
I have also added a schematic…
Part Number: UCC27714 I just like to know if I can separate the two ground on the UCC27714 ?
Meaning having the gound Vss connected to the microcontroller and COM connected to the power supply. This 2 ground would never be connected as I want to use…
Part Number: UCC27714EVM-551 Other Parts Discussed in Thread: UCC28951 , UCC28950 , UCC27714 , UCC28950EVM-442 , UCC28180EVM-573 , UCC27524 Hello,
I'm referencing on UCC27714EVM-551 to have input voltage 390 VDC converted to output 48 VDC / 10 A. Attached…
Part Number: UCC27714 Other Parts Discussed in Thread: UCC28C43 , Tool/software:
In a UCC28C43 + UCC27714 push-pull design:
Too short dead time : Cross-conduction risk → MOSFET temperature rise.
Too long dead time : Slower edges → Higher…
Part Number: UCC27714 Tool/software:
I designed the UCC27714 IC as shown below. I’m using the Rbias resistor as a short (0 ohms), and my Rboot resistor is 5 ohms. Everything else is the same as the schematic. However, I'm experiencing…
Part Number: UCC27714 Hello,
I have an issue with UCC27714 HO output. When running a pspice simulation, this IC works, when implemented in hardware the output stays at 0V while the LO output works OK. I have enclosed a snippet of my schematic. Thanks…