Hello,
The UCC28064 is typically designed for a minimum frequency of 50 kHz and a maximum of 250 kHz.
If you want to do a high speed design I would recommend using the UCC28065 instead that has a maximum switching frequency of 800 kHz.
You could design…
Hello Roberto,
The UCC28070 is the only analog interleaved-PFC controller from TI that operates in CCM.
TI has other interleaving controllers that operate in transition mode (TM) which can accept AC and DC inputs. Please consider the UCC28064A and UCC28065…
Part Number: UCC28180 Other Parts Discussed in Thread: TL431 , UCC28064A , UCC28050 , UCC2818 , UCC28056 , UCC28065 , UCC28070A Hi ,
I have implemened 1kW PFC stage as AC to DC with PFC Operation and its working good.
in my output 100HZ ripple component comes…
Hello Jim,
Newer PFC controllers with simulation models are: UCC28180 UCC28180 data sheet, product information and support | TI.com single-phase CCM UCC28056 UCC28056 data sheet, product information and support | TI.com single-phase TM UCC28070A UCC28070A data…
Part Number: UCC28070 Other Parts Discussed in Thread: UCC28065 , Got data sheet of UCC28065
Now I am designing LFP battery charger of 1650 watt(30A/54.8V).
After this, I want to design 350 watt and 3500 watt charger.
Perhaps, PFC will not be required for…
Hi Chandran,
Our UCC28070 is our only CCM interleaved PFC. We do have a series of transition mode (TM) interleaved PFC's with the latest being our UCC28065 . What is the power level and end application you are targeting?
hi Sachin,
if you set the Vo as 230V at calculator , then you can get the same result as app note.
by the way , UCC28065 is the latest two phase CRM PFC , you can consider to use it.
Part Number: LMG3411R150 Other Parts Discussed in Thread: UCC28065 , , LMG3410R150 Hi Team,
Customers are looking for 500W GAN total solutions Can we arrange concall with customer to introduce TI products to customers ?
UCC28065(PFC) + LMG3410R150(GAN) …
Part Number: UCC25600 Other Parts Discussed in Thread: UCC28065 , LMG3411R150 , LMG3410R150 Hi Team,
Customers are looking for 500W GAN total solutions Can we arrange concall with customer to introduce TI products to customers ?
UCC28065(PFC) + LMG3410R150…