Part Number: PCM1860-Q1 Other Parts Discussed in Thread: PCM1860 Hi expert,
From the Datasheet , we want to kown PCM1860-Q1 Support 4 channel or 2 channel?
Below the picture, we think it support 4channel.
But Below the picture, it seems just support 2…
Part Number: TIC10024-Q1 Hello,
I am planning to use the TIC10024-Q1 in an automotive ECU.
Since, as stated in the datasheet, the TIC10024-Q1 is designed and tested according to the ISO 16750-2: can I assume that it supports all the tests from the ISO…
Part Number: TDA4AL-Q1 Hi Expert,
What is the maximum camera resolution that MIPI CSI-2 can support? The datasheet says it is 4M? Because there are 2M*8 input at the same time, it should be 16M
If two CSI-2 are input at the same time, will the maximum…
The hardware checklist we have available is on Ti.com: https://www.ti.com/lit/pdf/sprad91
Regarding switching to USB micro-B connector - it should not be an issue assuming you have it pinned out correctly.
Part Number: TCAN1044V-Q1 Other Parts Discussed in Thread: TCAN1044AV-Q1 , Hi TRX team,
Could you provide test result of IEC 61000-4-2 for TCAN1044VDRQ1? My customer requests that data.
Kind regards,
Shota
Part Number: DRV8889-Q1 Other Parts Discussed in Thread: DRV8899-Q1 Hi
How to connect to 1-2 phases stepper motor ? motor spec as below. thanks!
2_Q24BJ48-XXXXW_0_0-00WX-1(1).pdf
Part Number: TDA4VM Hi TI team,
Currently we are developing a SIL-2 compliant product using TDA4VM. As per our current understanding in order to meet the SIL-2 requirement industrial grade component is fine and automotive grade(i.e part with Q1 extension…
Part Number: DS90UB960-Q1 Hi team,
What is back channel speed when paired with 935 and 935 works at CSI-2 no-sync mode? It must be 10Mbps? Can it be 50Mbps?
Thanks!
Jiawei