Hi,
Please make use of the attached design calculator to verify your design. There are tutorial links in the tool which helps you what to enter in each STEP.
Let me know if you have any questions on the tool.
5001.LM5069_Design_Calculator_REV_C…
Attach some files for reference.
1. dsi file and CSR file (Setting.zip)
2. Panel spec
3731.Setting.zip
6024B0250301_G070Y2-L01 ver 3.4 for Sturdy_C7_2017.pdf
Other Parts Discussed in Thread: UCD9248 We're bringing up a board with four UCD9248 parts. Excerpts from our schematics are available (privately) on request -- but it's a pretty standard design, borrowing verbatim from the Xilinx VC709 evaluation board…
Robert, I’m happy to say that the paper includes information for applications like yours. Here’s where to look.
Q1) TPA6132A2 can work very well to implement a pair of mono line drivers. See the schematic in section B.2 on page 11 of the paper, and…
Aaron,
In the TMS320C64x EDMA Architecture App Report SPRA994, Section 2.4 on page 6 says
"Only one TR from each priority queue can be serviced at a time by the address generation/transfer logic. The transfer logic can process transfers of different…
Part Number: MSP430FR5739
Hi,
I have purchased MSP430FR5739 recently. I have following questions would like to ask.
Firstly allow me describe my set up.
After I have downloaded program from USB, I disconnect usb and power the board from #1…
power off then on, 3rd sample and other is bad.logicdata.txt 1. As you (and data sheet) mentioned, /DRDY "returns high after the first falling edge of SCLK during a data read operation". Since /DRDY only has 1 channel to sample, perhaps it is staying…
Other Parts Discussed in Thread: LM5050-1 , TPS2490 , TPS2552 Many times a power design will have multiple inputs. Diode ORing is the term used to allow automatic selection of the input source.
Usually the diode that is shown is just a representation…
Part Number: DS90UB927Q-Q1
Hi team,
customer use 927+948, the LVDS and I2C can work normally, but the GPIO0-3 can't mapping and always low.
below is the 927 and 948 register setting, can you help to check it? thanks,
927
Fullscreen…