Part Number: TCAN1462-Q1
Hi Danny,
The customer wants to design this device of ISO 11898-2:2023 version on their board before June 2024, so please check the expected schedule and let me know.
Regards,
Hi Evan
Sorry for delay in response.
Getting power sources for ISO pulses is a hard job.
For now, we can provide a power source which is similar to ISO Pulse 1 and the functionality of device can be shown.
Thanks and Regards
Shiven Dhir
Part Number: DS90UB914Q-Q1 Other Parts Discussed in Thread: DS90UB926Q-Q1 , DS90UB913Q-Q1 , DS90UB953-Q1 , DS90UB948-Q1 Hello. I am designing a surround view camera system for automotive applications. I need to use a deserializer with two switching inputs…
Part Number: DS90UB941AS-Q1 Hello team:
Currently we have a product solution that use 1 941 to connect 2 948, to drive 2 screens and each one has touch.
According to https://www.ti.com/lit/an/snla308a/snla308a.pdf , Figure 10-4. INTB Logic in Splitter Interrupt…
Part Number: DS90UB935-Q1 Hi
My ISP outputs MIPI CSI-2 Continuous Clock mode to Serializer,
Is it necessary to configure the register 0x2[6] = 1?
It seems it works well with the register 0x2[6] = 0.
Thanks for your help.
Part Number: DS90UB954-Q1 Other Parts Discussed in Thread: DXP Hi, It's known that DS90UB954 can deserialize DS90UB933. But there is no csi output for DS90UB954 on the custom board.
(**) test log is as follows: (1) CSI_CLK0P/0N, DxP/N: keep 1.2V; (2…
Part Number: DS90UB954-Q1 Hi, team,
Please advise on my questions bellows:
Q1. Are there any equations which show the effective CSI-2 Output bandwidth of DS90UB954? I can find equations for the effective bandwidth on DS90UB960 data sheet, however, I cannot…
Part Number: LM5143-Q1 The use method is staggered single output, which is equivalent to 2 phases synthesized into a power output, 24V to 12V, and each phase output has an upper lower MOS tube, LM5143-Q1 quickstart design tool in the efficiency curve after…
Hi Jason,
OK, here's a dump of all my J784S4 EVM board of various registers using 9.0 U-Boot. Commands are from U-Boot prompt.
You should be able to get the dump/read the registers similarly on your setup as well.
PLL8
====
=>
=> md.l 0x688000…