Part Number: UCC2818-EP Other Parts Discussed in Thread: UC2854B-EP , UC2854 , UCC2818 Tool/software: Hi TI team
I would like to know which among these PFC ICs (UCC2818-EP and UC2854-EP) can have <5%THD on the input current for input frequency of 360Hz…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC2818 , UC2854 Tool/software: Hi TI team,
I have following requirements
Input voltage -100Vrms to 134Vrms
Frequency- 360Hz to 800Hz
output voltage- 400V
output power 100W
I am planning to UCC2818…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC28070A Hello,
I will rectify the 3 Phase 400 Hz 115 VAC input supply to DC (270 VDC) with the bridge rectifiers shown in the figure, and then apply boost PFC to 450 VDC with the UCC2818-EP integrated…
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC3817 Hello team,
Does TI have any available EVM which is able to evaluate UCC2818-EP?
EVM for other p2p PFC is also acceptable.
Regards,
Itoh
Part Number: UCC2818-EP Other Parts Discussed in Thread: UCC2818 Hi team,
Is it possible to use UCC2818-EP for three phase (400Hz) full-wave rectification AC-DC converter application?
My customer wants to design single/three-phase universal AC-DC power…
Part Number: UC2854B-EP Other Parts Discussed in Thread: UCC2818-EP , Hi,
The UC2854B-EP has the same functional bloc as UCC2818-EP, better current amplier bandwidth, low gain dispersion of multiplier but requiere more supply current and it is more expensive…
Hi Ray-san,
Are you referring to UCC28180, not UCC2818-EP ?
I searched UCC2818-EP datasheet but I didn't find the SOC spec you mentioned here.
Could you please double check?
Regards,
Itoh
Part Number: UCC2818-EP Other Parts Discussed in Thread: UC1854 , UC2854B-EP Hello team,
Does UCC2818-EP works in extremely low temperature condition (-54degC)?
I'm looking for generic PFC controller which works in -54degC condition.
Also, the PFC…
Part Number: UCC2818-EP Hello everybody,
I used the UCC2818-ep for an PFC flyback application.
To improve the mockup performances, I tried to configure the current loop but I constated that there is no impact on the Flyback behavior with all current…