Part Number: UCC28700 Hi Experts,
Seeking your assistance on this query:
I am looking at this schematic right now: https://www.ti.com/lit/df/tidrbq6a/tidrbq6a.pdf
In the UCC28700 datasheet I try to get the Rs1 and Rs2 values.
In the datasheet I can see…
Part Number: UCC28700 Hi,
I would like to know the changes that are necessary to make to get an output of 24V and 2A. I just need to change the resistances related to voltage sense in UCC28700, maintaining the same transformer, or do I need to change…
Part Number: UCC28700 Other Parts Discussed in Thread: PMP40144 , UCC28704 Hello,
I want to use this IC to generate 12V from a 48V DC supply. But on the WEBENCH I am not able to give 48V in the input range. Is this IC limited to 85 ≤ value ≤ 265 input voltage…
Part Number: UCC28700-Q1 Hi,
Where could I get the data of the amount of integrated transistor in UCC28700QDBVRQ1?My customer want to count the Fit.
Thanks a lot!
Part Number: UCC28700-Q1 Other Parts Discussed in Thread: UCC28700 , Hello Folks,
I have a question regarding the control of the UCC28700. First I would like to tell our application. We are using the controller as main power supply for our application…
Part Number: UCC28700-Q1 Other Parts Discussed in Thread: UCC28700 Hi,
I use the UCC28700 for a flyback 12V3A and the WE 7508112341 trafo.
i cant reacht the max output current, after 1.6A the voltage drops slowly to 0V, it seems like a current limitation…
Part Number: UCC28700-Q1 Other Parts Discussed in Thread: TIDA-01604 , UCC28700 , Hi, support team
My customer has the questions as follow:
I have gone through TIDA-01604 design
1. Is it possible to design 7.2KW?
I need to convert 220vac, 50hz to 700vdc…
Part Number: UCC28700
Hi experts: Regarding the application of UCC28700, customer have a few question, could you help us on that?
1: The pspice model customer downloaded on TI's official website cannot be simulated with orcad capture. It always reports…
Other Parts Discussed in Thread: UCC28700 Hi,
I am trying to design flyback SMPS for an input of 240V and output of 25V, 1.2A. I have used web bench power supply design to generate a circuit. I have created similar circuit in TINA. But I could not able…