Part Number: UCC28730-Q1 Other Parts Discussed in Thread: UCC28730 Tool/software: Hi Team,
We are facing an odd problem. We found the frequency of the UCC28730 output is not as expected. According to the datasheet, the max switching frequency should…
Part Number: UCC28730-Q1 Other Parts Discussed in Thread: UCC28730 Hello,
Regarding the controller UCC28730-Q1, I have another 2 concerns:
1. In order to keep the stability in all the operating range, it is indicated the next equation of Cout (Ecuation…
Part Number: UCC28730 Tool/software: Hi TI,
There are a few questions about UCC28730.
1. In previous post, there is a reply which mentioned " If you do this in your design at maximum load the switching frequency will be 70 kHz at no load the switching…
Part Number: UCC28730-Q1 Tool/software: We are designing our Flyback circuit with 400Vin and 18Vout, 13W using this controller.
I have used datasheet to calculate Rcs,
for an efficiency of 85% and ηxfmr of 91%, Nps = 6; Rcs can be calculated from…
Part Number: UCC28730
Hello,
Where can i found the Spice model of :
UCC28730 and UCC24650
i need the spice model in order to simulate a circuit on Altium, there is only the encrypted version.
Thanks
Other Parts Discussed in Thread: UCC28730 , TINA-TI Tool/software: There is no generate part option under the "tools". So I tried to use "New Macro Wizard" to import UCC28730 spice model. I pick the netlist file to generate it but it gives me "Invalid…
Part Number: UCC28730-Q1 Other Parts Discussed in Thread: UCC28730
Tool/software:
Hi,
One of the reference designs for UCC28730 shows HV pin pull resistance of 900k for 60V-1000V Vin. (Refer image)
According to datasheet, the start-up current…
Part Number: UCC28730-Q1 Dear Team,
Customer has been analyzing the UCC28730-Q1 datasheet, and raised some queries regarding the control. Please, can you give us your feedback?
VCCR parameter
Datasheet: “The term VCCR is the product of the…
Part Number: UCC28730-Q1 Other Parts Discussed in Thread: UCC28730 Tool/software: Hi Team,
I would like to know is there any possibility if added circuit to can control the line voltage precisely about 50 +/- 3V using UCC28730-Q1
Below is the…
Part Number: UCC28730-Q1 Tool/software: I have designed a 23 W Flyback-Converter with 1Outputs with a Inputvoltage of 250-800V and an Outputvoltage of 11V/2.1A. I am now trying to put the PCB in operation, but I am facing unstable switching behaviours…