Hi Robin,
Please send to my email bryce-xun@ti.com
robin gangopadhya18 said: TPS55288 is I2C controlled by WT6636.
( or preferably by a TI chip)
You can post a thread to ask if there is a suitable TI PD controller for this, I think there should be some…
Part Number: UCC28782EVM-030 Other Parts Discussed in Thread: UCC28782 , TPS55288 , TPS65987 Hello:
We will greatly appreciate if a correct circuit-based explanation is provided for the series switch shown in the referenced 2016 TI publication named "Evolution…
Part Number: UCC28782EVM-030 Other Parts Discussed in Thread: TEST2 Hello:
Following up on the last post regarding Direct drive with Diff opamp, pl see the DC Decoupled version.
Will this work: if it does, what will be the opamp output characteristics…
Part Number: UCC28782EVM-030 Hello:
Wondering if it is possible to inject the small signal while setting up an SMPS for loop gain-phase measurement with a nonisolated opamp for its broadband properties but of course, the limiting factor is the output…
Part Number: UCC28782EVM-030 Hello Mike:
What would be your explanation for the theory of allowing to use of the same nodes to measure loop response as Vout/Va as the nodes where the signal is injected with floating nodes from the transformer?
Therein…
Part Number: UCC28782EVM-030 Other Parts Discussed in Thread: ATL432 , UCC28782 , TL431 Hello:
Pl see attached ppt copied from the EVAL kit document.
The table shows how Rdm & Rtz change with load.
How does one interpret the Table?
It is clear that a…
Part Number: UCC28782EVM-030 Other Parts Discussed in Thread: UCC28782 , ISO7710 PL SEE ATTACHED.
Wondering if the document needs to be updated.
r iso7710delay.pptx
Part Number: UCC28782EVM-030 Hi team,
I know we can use type-c PD to achieve different Vout (5V/9V/15V/20V), but how to judge the OVP can be latched at different Vout?
BR,
Jimmy
Part Number: UCC28782EVM-030 Other Parts Discussed in Thread: UCC28782 , , ATL432 Hello:
We have some UCC28782 based modules: assembled with values close to the UCC28782EVM-030 EVAL KIT. Right now, input is rectified AC with sufficient input filter and…
Part Number: UCC28782EVM-030 Hello
We made a xmfr 40:8:8
Which should have reduced Bac 60%, thus hopefully, DC bias value.
But it did nothing to reduce core temp. We ran 100W ...stopped when inside the core temp went up to 130 deg C.
Temp rise is not…