Part Number: UCC2895 Hi Sir,
I am testing this controller if i direct turn on the input the controller pulse is getting off and in output voltage ripple is more
Part Number: UCC2895 Hi Experts;
I am currently facing a problem regarding the output voltage. Nearly all test conditions are normal but when I increased output power, up to 3300watt for instance, the output voltage drops approximately 10-20V. In other…
Part Number: UCC2895 Other Parts Discussed in Thread: UCC3895 , Hi team is it possible to adjust the output voltage by injecting a current with a resistor by applying a DAC to the feedback connection of ucc2895/ucc3895?
Note ; the controller is on the primary…
Part Number: UCC2895 While the soft start pin voltage rises from 0v to 5v for about 1 sec, the maximum duty is about 0.7v.
At this time, an overcurrent trip occurs, what should I do?
Part Number: UCC2895 When the output is short-circuited (CH1), the waveforms of SS pin (CH1) and CS pin (CH2) are as follows, CS pin tops to nearly 2V and then returns to 0V. look at the SS pin from high to low but cannot recover. Want to know if there…
Part Number: UCC2895 Dear Sir
Attatched the Pin 13 & Pin 14 's waveform .
The following 13 - and 14-pin theories should be complementary. Under what circumstances will the overlapping uncertain states in the figure appear?
Sch:
A811AV07A.p…