Part Number: UCC28C43-Q1 Hello,
I made a Flyback converter with the UCC28C43-Q1 but I use an external error amplifier.
Can I put to GND "FB" Pin and overwrite the output with the external "Comp" signal?
Thanks in advance!
Best regards…
Other Parts Discussed in Thread: TPS40210 , UCC28C43 , UCC28C55-Q1 Hello Team,
I want to design the power supply with below specification.
Input : 48V
Output : 3500Vdc, 3mA
Protection : Overvoltage, Overcurrent, short-circuit.
Isolation : Yes
Also I need…
Part Number: UCC28C43-Q1 I am Trying to compensate the model UCC28C43-Q1 but i cannot find the spice average model on ti.com.
Can you please share with me the average model so i can make the further analysis?
Part Number: UCC28C43-Q1 Hey, i wanted to know that does the tina spice startup model given on ti.com have a zener across the PWM controller ?
Because while performing the overcurrent protection simulations, I am not able to get proper results.
I hope…
Part Number: UCC28C43-Q1 Hi team,
Could you please share the FMEDA file of UCC28C43QDRQ1 so that my customer can use it to do system level analysis? You can reply to me through emails. Thanks.
Part Number: UCC28C43-Q1 Other Parts Discussed in Thread: TIDA-01505 Hello,
for a DCDC converter design we use this TIDA-01505 as Reference. IC and transformer are the same.
After anaylsing the design description and datasheet a few Questions are still…
Part Number: UCC28C43-Q1 Other Parts Discussed in Thread: UC2843A-Q1 , TPS92692-Q1 , TPS92691-Q1
How can I use current mode PWM controllers or LED drivers in an automotive high-voltage contactor economizer?
A high-voltage electric battery in HEV/EVs is…
Part Number: UCC28C43-Q1 Other Parts Discussed in Thread: UCC28C43 My customer are using UCC28C43-Q1 for EV/HEV PTC application.
specs: Flyback isolation application
Input: 150-500V DC.
Output: 15V/0.33A=5W.
Now my customer want to add input over voltage…