Part Number: TPS2812 sluu139.pdf
Figure 1
How are the RC parameters of the two snubber circuits (R20, C16, R21, C17) of the push-pull converter in Figure 1 taken? How to calculate the power consumption of R in the snubber circuit?
In addition…
Part Number: UCC38085 Other Parts Discussed in Thread: UCC256402 Hello,
I am trying to make open loop simulasion for a LLC circuit. I am confused at some point. I am designing my half bridge LLC converter for a specific output voltage of 12V at 250W…
Part Number: UCC38085 Spec : 1.Vin=42V
2.Vo= 24V
3.500W DC-DC Converter
Can you provide two solutions? THX
1. DC-DC Converter + GAN +SR
2. DC-DC Converter + MOS +SR
Part Number: UCC38085 Hello Guys,
Good day.
Our customer just like to clarify what the the voltage source Vbat that is connected to the Vdd pin of UCC38085 means. Is this a battery? What type of battery is this?. See below image.
Thanks for the clarification…
Part Number: UCC38085 Other Parts Discussed in Thread: TPA3255 , G'day team.
I'm doing a large project using 3 x TPA3255 s which is a mains/portable public performance amplifier system. The 'portable' part is where I need a bit of assistance.…
Part Number: UCC38085 Hi FORUM.
I am now working on a DC-DC converter using the 38085 but there are a couple of things in the Data sheet which are not very clear to me.
The value of this resistor is found from the Formula on the image. I'm not too clear…
Hello Teng,
I would like to know if your colleagues could help me with my questions? Do they know why the current sense gain is missing in the current sense resistor calculation guide (TI application note: http://www.tij.co.jp/jp/lit/an/slua584a/slua584a…
Part Number: UCC28083 Hello everyone,
I am designing a current sense resistor so that I can use it in the Current mode controller UCC28083 ( http://www.ti.com/lit/ds/symlink/ucc38085.pdf ). The inconsistency that I have found is that in the aplication note…