Part Number: UCC5870-Q1 Hi experts!
I cannot find the Rint (gate driver internal gate resistance) value required in equation 4 of the datasheet to compute the total device power dissipation.
If I use the XL Calculator Tool I see different values of equivalent…
Part Number: UCC5870-Q1 Other Parts Discussed in Thread: UCC5871-Q1 , What are the specific differences between UCC5870-Q1 and UCC5871-Q1? Do you have the latest product models in the same series?
Part Number: UCC5870-Q1
Hi Expert
we have five question as below:
1. can we choose below way to design the OUTH and OUTL driver resisters?
2. what difference between VCECLP and DESAT?
3. if we needn't AI2~AI6, How to connect it? pie to GND?
4. what…
Part Number: UCC5870-Q1 hi expert
from my understanding to Viso, this parameter represents Maximum AC r.m.s . isolation voltage for one minute.
for UCC5870-Q1, the Viso is 3750v.
I have two questions.
Q1: if we use 3860V DC to test UCC5870, it will damage…
Part Number: UCC5870-Q1 Is there a time-out which triggers a sample on internal ADC? Or must the IN+ pin see a transition to get a new sample? Or could it be triggered some other way?
Is there a common or recommended way to trigger externally, say as…
Part Number: UCC5870-Q1 hi experts
i have two questions about Rpui and Rpdi.
Q1: do the parameter of Rpui and Rpdi mean the internal resistor in UCC5870?
Q2: whether can some configurations for UCC5870 registers affect these parameters real value?
some…
Part Number: UCC5870-Q1 hi experts
i see the following configuration in UCC5870 datasheet.
My question is that 0x0 or 0x1 means not repot this fault to nFLT1?
Part Number: UCC5870-Q1 Hello
I have a problem that I encounter to perform some DC tests of the UCC5870 driver.
After carefully performing the test configuartion, indicate in the EVM user’s guide. We are not able to display the signals generated by the…
Part Number: UCC5870-Q1 We are using the UCC5870-Q1 and are getting an STP_FAULT [STATUS2 bit 11] when changing the ASC_EN state.
The scenario occurs when: * ASC_EN is at a high level * ASC is at a low level * IN+ is at high level * IN- is at a low level …
Part Number: UCC5870-Q1 HI expert
i have question about Vceclp function
if customer don't use Vceclp pin, can they float this pin ?
What impact this will have?