Part Number: UCC5871-Q1 Hi Expert,
For the application of ucc5871-Q1, we have some issue. As the picture showed below, When the short circuit happens, we will open the SIC-MOSFET, there will be a high voltage at Vds of MOSFET because of parasitic loop…
Part Number: UCC5871-Q1 If we drive the SiCMOSFET with 18V and -5V from ucc5871, can the Miller clamp protection function active?
And from the pic above, What is the ground for ISTO, is it VEE2?
Part Number: UCC5871-Q1 hi expert
i find the following picture from datasheet about DESAT function.
i have a question about tleb. from my understanding, the begin of tleb is rise edge of OUTH as quick calculation tool shown(tdesatleb), am i right?
do…
Part Number: UCC5871-Q1 Hi team.
My customer plans to use UCC5871-Q1 to driver SiC MOS instead of pyrofuse for faster react time, and in their configuration there's only one FET. I'd like to check with you:
If not bridge configuration, customer…
Part Number: UCC5871-Q1 Hi Experts,
We would like to know the minimum and maximum R(ON) resistance of the gate driver IC.
Seems the information is not available from datasheet.
Regards, Archie A.
Part Number: UCC5871-Q1 Dear team,
If these two pins ASC_EN & ASC are not used, they should be connected to GND with pulldown resistors in my understanding, right? What is the recommendation for the pulldown resistor? Is it ok to use 1kohm?
Thanks &…
Part Number: UCC5870-Q1 Other Parts Discussed in Thread: UCC5871-Q1 , What are the specific differences between UCC5870-Q1 and UCC5871-Q1? Do you have the latest product models in the same series?
Part Number: UCC5871-Q1 Dear team,
Can VCECLAMP trigger continuously? Customers want to configure lower Roff drive parameters to reduce losses. Trigger VCECLAMP in the peak current region (30s each time, the total time is not limited), so as not to exceed…