Part Number: UCD90160A Hello, Team
our customer would like to know which our function support "on the fly" change?
which means no need to power cycle when new setting take action.
Part Number: UCD90160A Hello, Team
we`d like to check our UCD90160A VOUT_COMMAND (0x21) registor,
would it matters if we disable the Closed-Loop Margining mode?
Part Number: UCD90160A Hello,
Is it possible to use USB-TO-ANY instead of USB-TO-GPIO to programm UCD90160A with Fusion Digital Power Design?
Thank you.
Best regards,
Kübra
Part Number: UCD90160A Hello expert,
My customer would like to know if there is VCC detect function. Can UCD90160A record it's own Vcc(3.3V) power fault and provide to BMC the next power cycle? if yes, what's the method we need to implement? Thanks a…
Part Number: UCD90160A Hi,
When using the 16-Rail Power Supply Sequencer it says in this devices data sheet that it possess 26 GPIO pins. I want to use the GPIO pins as power supply enables. However, there are only 16 rails available in the GUI how can…
Hi,
I wanted to ask that can a Project file(.xml) from a UCD90160A be used on a UCD90160 part. Since I have a config file from the A part and which to import it into the GUI using a non-A part.
Part Number: UCD90160A My UCD90160A design seems to be measuring all rails like they are very choppy, going up and down like 5-10%.
I don’t have a ferrite filter for the analog rail, and the common digital rail has some 11mV switching noise on it.…
Part Number: UCD90160A Hi TI service team,
I have some questions about UCD90160RGCR Brownout function and also attach my calculation of capacitors application on my board.
*C (brownout) = (80mA*5ms) / (2.9V-2.6V) = ~1334uF, 1334uF*1.2 = 1600uF (20% margin…