Part Number: UCD90160A Hi Team,
The customer got an enquiry about UCD90160ARGCR GPI response time.
In this particular project, they are using pin 32 “GPI2” as input pin to monitor thermal-Trip-L from the MCU.
Below is the waveform they captured…
Part Number: FUSION_MFR_GUI It appears that the link to download: https://www.ti.com/tool/FUSION_MFR_GUI is broken. A related link included in a previous report of the same issue a few years ago is also no longer valid or works
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90160 ,
Dear team,
As SLVA908, project file generated from UCD90160 devices can be seamlessly imported into A version.
Does project file of 90160A can also seamlessly imported to non-A version…
Part Number: UCD90160A Hi,
I have the UCD90160A power sequencer in a JTAG chain.
However I am having some problems getting it to report its ID code when scanning the chain.
I can confirm it is going into JTAG mode, as the PMBUS address changes to 126…
Part Number: UCD90160A In reviewing this project that came from another engineer,... we noticed the setpoints for over/under fault is 15%, the over/under warnings are 10%, and margin Hi/Low is 5%.
I am unclear on what the "margin" actually does and how…
Part Number: UCD90160A On the UCD91060A which pin is considered the "CONTROL pin" mentioned below in the FAQ
********
"The correct method to sequence off rails is to use the CONTROL pin. A delay and dependency configuration of each rail is observed…
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90124A Hi expert,
My customer want to use s equencer and they want to know something about Clock/data rise time and fall time(tr and tf).
UCD90160A DATASHEET: max Tr is 120ns
UCD90124A DATASHEET…
Part Number: UCD90160A A similar question has been asked before about the Offline version and the answer was that the Export function is not available in the Offline software only the Live mode. Well I am running in Live mode and I do not see the export…
Part Number: UCD90160A
Hi Team,
What is the PMBUS command(s) needed to read the analog voltage inputs on the UCD90160A (if possible, looking for MON1-16)?
Regards, Diego
Part Number: UCD90160A Question about "Fusion Digital Power Designer" (aka FDPD) - no access to "Export" function
Details:
Have FDPD version 7.7.1 installed, USB Adapter attached (firmware rev 1.0.11) but UCD90xx device is NOT connected…