Part Number: UCD9081 Hello,
we are reading the error log by reading 48 bytes from address 0x1000, but we have no idea how to interpret this. it also doesn't seem to give us the complete error log.
Is there a document that explains how this information…
Part Number: UCD9081
Hi,
1. What is the recommended for choosing the UV/OV Threshold?
2. Suppose I have a 2 power supplies with 1.0V and 3.3V, is the UV/OV Threshold need to be according the present % like 5% UV and 5% OV or like 150mV_UV and 150mV_OV…
Part Number: UCD9081 We’re trying to toggle the GPOs on the UCD9081, and we are having some trouble decoupling the GPO output toggles from the power sequencing.
Instead of trying to toggle the GPOs upon boot up, we want to control them through I2C…
Part Number: UCD9090A Other Parts Discussed in Thread: UCD9081 , Hi team,
It's the first time for my customers to use UCD9090A/UCD9081, they have below questions, need your kind answers.
1. What are the 8 digital inputs of UCD9090A? Is this function same…
Part Number: UCD9081 Other Parts Discussed in Thread: UCD9080 I want to use the Fusion Digital Pwer designer tool in the offline mode to create a new project. Since this is a new design I want to develop it in off line mode.
The UCD9081 device is not…
Other Parts Discussed in Thread: UCD9081 , UCD9080 Newbie to the forum, need some pointers from the experts.
Where I can find spice model for UCD9080 & UCD9081.
Thank you.
Fred
Part Number: UCD9081 Other Parts Discussed in Thread: UCD9090A What is the maximum power this component can handle?
What does operating free air temperature of 85C means? How does it relate to max junction temperature?
What is the max junction temperature…
Part Number: UCD9081 My UCD9081 is keep on Resetting my system. I want to understand what is going wrong on the device.
Expecting to have a call to review the design.