Part Number: UCD9246 In the newer GUI (7.0.18) I can't find where to set the turn on and stay on dependencies when setting up the UCD9246 controller.
Where are these settings hiding? I think these are related to the GPIO_SEQ_CONFIG PMBUS command, and…
Other Parts Discussed in Thread: UCD9246 Customer is using UCD9246 and Fusion Digital Power, but Vout was not output.
I think that the reason is UCD9246 firmware version.
customer is using UCD9246 ver 5.6.0.xxxxx, but attached document is described ver…
Part Number: UCD9246 This device is programmed at ICT (InCircuit Test) prior to bringing up all power rails. It appears that the device programs on the very first attempt. All subsequent programming attempts fail. After a few attempts the device is no…
Other Parts Discussed in Thread: UCD7242 , UCD9246 Customer has problem occurred for UCD9246 and UCD7242 below.
・FLT flag is asserted for once every few month(~6 month).
※Overcurrent and temperature have big margin, these are no problem.
If there past…
Customer hope to set non-function FLT input for GUI register only setting.
I think that two below idea is match, is it correct?
①Configure→Iout,Vin,Temp Config→Fault Response
⇒Continue Without Interruption
②Configure→GPIO Config → FLT…
Other Parts Discussed in Thread: UCD9246 , UCD90120A Please let me know about start up time (please see below) of UCD90120A & UCD9246.
Between; Supply voltage input ⇒ Set the resistor ⇒ Start output control
Best regards,
Satoshi
Hello,
can someone tell me where I can download the " 5.14.0.12640" firmware update data file to perform a fusion tool firmware update on the UCD9246?
Thanks
s
Other Parts Discussed in Thread: CDCE62005 , CDCE62002 I am using CDCE62005 and CDCE62002 in my design. ( http://www.ti.com/lit/ds/scas862d/scas862d.pdf )
Page 70 starts a discussion of thermal management. Page 71 shows the recommended internal via configuration…
Other Parts Discussed in Thread: UCD7242 , UCD9246 Hi,
I designed a board with PWM controller (UCD9246) + two (UCD7242), It is designated for four output voltage, three rails of voltages are working well, I can see different ranges of output voltages (0…