Part Number: IVC102 Hello, I'm designing a circuit that uses the the IVC102 with an unbiased photodiode. Similar to the circuit shown in the datasheet below:
The datasheet mentions the minimum negative supply voltage (V-) needs to be -10V. However…
Part Number: TPS54561-Q1 All simulations for a power supply I was redesigning failed. I tried to redo a simulation on one of my previous designs (without any change) and it failed too. I believe the server running the simulations is down.
Hi Nicolas,
Take a look at the LM5145 EVM, as it's a 2-sided design with controller underneath. The LM5145 is effectively the same controller, just with a reduced Vin-max rating of 75V.
Regards,
Tim
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS62825 Not sure where to report problems with WEBENCH, so I'll do it here.
I'm getting an error when I try to export design files from a WEBENCH design. This happens on all part…
Part Number: LM3478 While playing around with design parameters for a LM3478 design, I noticed that Webench's SEPIC schematic and Boost schematic differ in the placement of Cfilt for monitoring Vsense at the Isense pin.
Boost:
SEPIC:
Note that…
Hi Stephen Ziel and Patrick Yao ,
I managed to obtain the part number of the component I used, which is LM27762DSSR. Unfortunately, it couldn't generate 12V at the output, but the option they gave me is the one I'll go with. I'll start my design with the…
I am closing this thread since I have not heard from you for sometime. If you are still trying to resolve the issue, please feel free to open a new thread. Thanks - EL
Part Number: LM5160 Hey Buck Regulator team,
I have a customer working on a power tree for a new design and we were hoping your team could provide some guidance. Please see a summary of the input/output requirements below in addition to some questions…
Part Number: LMR51450 I am trying to build a circuit where I will get 22.V at the input and 12V 5A at the output using LMR51450. The circuit I built by reading the datasheet is attached. I want to compare the circuit I built on Webench, but it automatically…
Part Number: TPSM8D6C24 Other Parts Discussed in Thread: TPS546D24A Customers are verifying the TPSM8D6C24 configuration with Fusion Digital Power Designer.
(Substituted with TPS546D24A)
As configure the settings, the Compensation part will change to…