Part Number: WL1831MOD Other Parts Discussed in Thread: WL1835MOD , WL1837MOD , , WL1835 Hi,
My customer has issue with supply chain of WL1831MOD and would like to see if supply chain of WL1835MOD and WL1837MOD can be better.
But he is not aware of differences…
Part Number: WL1831MOD Other Parts Discussed in Thread: WL1271 Kernel: 5.14.2 from RT tree
Platform: Elkhart Lake
kernel parameters: root=/dev/ram0/ rw idle=poll cma=160M@0-2G pci=pcie_bus_perf sdhci_pci.max_freq=50 console=ttyS6,115200 console=tty0 dyndebug…
Part Number: WL1831MOD Hi Team, seeking some clarifications.
Do we have related devices that are Wifi6 compatible? Does this implies that we have WPA3 Security feature?
Thank you.
-Mark
Part Number: WL1831MOD We are streaming via WIFI (~10Mbps) and if we start a bluetooth audio stream concurrently we experience bad quality on the bluetooth audio stream. We are on the newest firmware. Can you give an idea how to track down the problem…
Hi Neil,
This error is occurring because you are trying to open two UART instances to the same COM port (Tera Term and HCITester). You can only have one open at a time.
I recommend using HCITester to generate the HCI commands you need first. Next, save…
Hi Mitch,
I generated an hcitool command from the picture you sent above. It looks nearly identical, except the length specification is 0x00 instead of 0x01. Can you try this value instead?
Mitch Neeld said: hcitool -i hci0 cmd 0x3f 0x106 0x01 0x00 0x01…
Part Number: WL1831MOD Other Parts Discussed in Thread: WL1831 Hello all,
We have an equipment issue on several cards where the WL1831MOD has its WLAN IRQ pull-up equipped (was supposed to be "not installed").
So the WL1831MOD is running permanently…
Part Number: WL1831MOD Hi, support team
My customer has the questions as follow:
Please help me find a replacement WL1831MODGBMOCT in stock.
Thanks so much.
Best regards, Yuki
Seyed,
Reviewing our BT Spec, I see that SPP depends on RFCOMM and L2CAP - Looking further you can see that the optional feature of extended window size larger than 23 octets is not supported.
https://launchstudio.bluetooth.com/ICSDetails/85355
So my…
Part Number: WL1831MOD Other Parts Discussed in Thread: WL1807MOD , WL1837MOD Hi Team,
Good day.
Can you please confirm if the WL1831MOD {WiLink 8 industrial Wi-Fi, Bluetooth & Bluetooth Smart (Low energy) module} is industrial grade also even its temperature…