Hi Ryan,
Please state the SIMPLELINK-CC13X2-26X2-SDK version you are evaluating.
The SDK version is simplelink_cc13x2_26x2_sdk_4_10_00_78 .
When adding endpoints do you modify the Zstackapi_bdbRepAddAttrCfgRecordDefaultToListReq API parameters?…
Hi Samrudhee,
Please see my comments below
1. This is part of the functional safety documentation we provide and can be accessed from ti.com. Please request for the same in https://www.ti.com/product/DRV3901-Q1#tech-docs
2. Please see the attached…
Hi,
the ISO124 has a small signal bandwidth of 50kHz. This is way too slow to measure electrical fast transient burst (EFT, IEC61000-4-4).
4_Transient_immunity_testing.pdf
Kai
Hi Paul,
Yes, I have the --gcc option select. So, the default of the CCS 4.0 support it.
How to determine the TI ARM compiler version 4.6.1 from CCS 4.0?
Thank you Mike
----------- Build CCS 4.0 configuration settings ---------------- …
Part Number: TDA4VM
Hi TI,
I am debugging a gpio driver in J721E, I found a curious problem, when I compile the driver as .ko, and insmod, it works well, but when I build it into kernel, the kernel will always can't get the gpio number, calling API…
Hi,
I mean I can play it in VLC, but it play not smoothly. when I use the Elecard StreamEye Tools to play it , it is smoothly, i
I have uploaded the video . Because i want to upload the video ,so i have to change the file`s expanded-name to txt, it…
Part Number: LM25066A Other Parts Discussed in Thread: LM25066 Hi team,
I am still in the process of getting some scope shots, but my customer has been using the LM25066A and having problems. They have implemented it exactly like shown in this design…
Part Number: TDA4VM
Hi Team,
I am using the below onnx model. Please rename the file to pfld.onnx
This is a face landmarks model taken from open source.
pfld.onnx.txt
The TI SDK version I am using is 8.1
When I tried to import the model…
Part Number: LM5069 Hi team,
Custome feedback that some of board is no output at LM5069.
What's the suggestion check point?
They change Ctimer but no different.
Good:
Issue:
Thanks
Shaq.
Brandon_LM5069_Design_Calculator_REV_C…
Part Number: TDA4AL-Q1 Tool/software: Hi,
Linux SDK: ti-processor-sdk-linux-adas-j721s2-evm-09_02_00_05
I am debugging CSI2RX IF driver in our own product based on TDA4AL platform, and I encountered below issue when I using below dts configuration…